The following command-line options are supported by the Sourcery CodeBench Debug Sprite:
-b Print a list of board-file
files in the board config
directory.
-h Print a list of
options and their meanings. A list of
device-url syntaxes is also
shown.
-i Print a list of
the accessible devices. If a
device-url is also specified, only
devices for that device type are scanned. Each supported device
type is listed along with the options that can be appended to
the device-url. For each discovered
device, the device-url is printed
along with a description of that
device.
-l [host]:port
Specify the host address and port number to listen for a GDB
connection. If this option is not given, the Debug Sprite
communicates with GDB using stdin and stdout. If you start the
Sprite from within GDB using the target remote |
arm-none-eabi-sprite ... command, you do not need this
option.
-m Listen for
multiple sequential connections. Normally the Debug Sprite
terminates after the first connection from GDB terminates. This
option instead makes it listen for a subsequent connection. To
terminate the Sprite, open a connection and send the string
END\n.
-qDo not print any messages.
-vPrint additional messages.
If any of -b, -i or
-h are given, the Debug Sprite terminates after
providing the information rather than waiting for a debugger
connection.